Search FAQs
Does the ATV61/71 jog function require a run command to work?
Issue:
Jog function requirements on ATV61/71
Product Line:
Altivar 61/71
Environment:
All models and serial numbers
Cause:
The Jog will not start when the assigned logic input goes high.
Resolution:
When the JOG function is activated, the VFD still needs a run command input to run the motor.
Jog function requirements on ATV61/71
Product Line:
Altivar 61/71
Environment:
All models and serial numbers
Cause:
The Jog will not start when the assigned logic input goes high.
Resolution:
When the JOG function is activated, the VFD still needs a run command input to run the motor.
Released for:Schneider Electric Global
Explore more
Explore more