Browse FAQs

What are the Twido Compact power supply specifications?

Published date: 04 September 2018

The following table provides power supply information for the Compact controller.

ITEM
SPECIFICATIONS
Power supply voltage Rated power voltage; 100 to 240 vac.
Allowable range; 85 to 264 vac.
Failure - depends on quantity of used inputs and output points. Generally, failure is detected when voltage drops below 85 vac, stopping operation to prevent malfunction.
NOTE: Momentary power interruption for 20 ms or less at 100 to 240 vac is not recognized as a failure.
Inrush current flow at power-up TWDLCAA10DRF and TWDLCAA16DRF 35 Amp maximum
TWDLCAA24DRF 40 Amps maximum
Power supply wiring UL1015 AWG22 (0.64 mm) or UL1007 AWG18 (1.02mm) Make the power supply wiring as short as possible.
Ground wiring UL1007 AWG16 (1.30 mm) Do not connect ground wire in common with ground wore of motor EQUIPMENT.

Note: The Twido is obsolete and has been replaced with the M221, for more information on this contact your local distributor or Schneider Electric sales.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.