Browse FAQs

SCADA 7.20 system starts however no device can communicate

Published date: 07 November 2018

Issue
When PLSCADA 7.20 is started, the runtime will start and client will display however no device information is displayed....only system errors "Server could not be located"

Product
PLSCADA 7.20 (PSE)

Environment
Windows Server 2008 with Data Execution Prevention (DEP) enabled.

Cause
Data Execution Prevention is a security feature of the CPU that prevents an application from executing code from a non-executable memory region. This will cause aspects of PLSCADA to crash

Resolution
Disable DEP:

1) Open Control Panel
2) Click on System and Security -> System -> Advanced system settings.
3) In the Advanced tab, click on the Settings button in the Performance section.

4) In Performance Options, select the Data Execution Prevention tab. Here you can turn on DEP support for Windows essential programs and services only or for all programs, with the possibility to define exceptions for non-compliant software.

Select "Turn on DEP for essential Windows programs and services only"


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.