{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.
 

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Search FAQs

BMENOC03x1 Maximum Server Connections

Title
BMENOC03x1 Maximum Server Connections
 
Issue
BMENOC03x1 Maximum Server Connections increase
 
Product Line
M580
 
Environment
Control Expert or Unity Pro

Resolution
 As of firmware version 2.08, the BMENOC03x1 now allows the below maximums regarding Server connections:
EtherNet/IP (CIP explicit messaging): server simultaneous requests is 32 or Modbus TCP (Modbus explicit messaging): server simultaneous requests is 64.
 
Explore more
Explore more