Thailand
Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website for company information.

Select your location
  • Default Alternative Text

    Easier access to clean water

women at clean water collection site

Challenges

Today in remote villages without energy, people spend approximately 1/3 of their time managing their water needs for domestic or agricultural use. 

You want to simplify access to water in remote villages without energy access. Water will be easily accessible thanks to automatic solar pumping.
  • Solutions

    With the Water of the Sun system, Schneider Electric provides a fully automatic solar powered water pumping system. The system can pump in a well up to 200 meters without any battery, relying 100% on solar energy and adapting its pumping intensity to the sunshine available.
  • Value Proposition

    Water of the Sun provides continuous water supply. It is compatible with grid mains supply and a wide choice of pumps and solar arrays available on the local market. It works 100 % with renewable energy. This solution is easy-to-install and maintain.
  • Differentiation

    • Tested and validated architecture relying on best-in-class Variable Speed Drive solution from Schneider Electric 
    • Software programming is easy to install and maintain
    • Technical support from Schneider Electric in more than 100 countries
Men working on renewable energy solar panels and Schneider Electric water tank

100% solar or hybrid solution

Water pumping for domestic use and/or irrigation purposes in areas with no grid power or erratic supply of power from grid.
Optional water treatment unit.

Benefits

  • Schneider Electric clean water collection station
    • Easier access to water
  • women at clean water collection site
    • Access to a clean water
  • Smiling woman rowing a boat for transportation, urbanization.
    • Business generation: clean water sales