วันนี้เราสามารถช่วยคุณได้อย่างไร?

How to Configure the Autorecloser on PowerLogic P3 protection relay

Issue

Customer wants to know how to configure the autorecloser function on a PowerLogic P3 device.

Product

PowerLogic P3 protection relays

Environment

Protection configuration – Autorecloser (AR) settings

Cause

The customer requires guidance on where to find official instructions for setting up the autorecloser function.

Resolution

To configure the autorecloser on a PowerLogic P3 device, refer to the official Schneider Electric application note.

Download the document ANGEN.EN005, which provides detailed steps for configuring the autorecloser feature.

You can access the application note using the following link:
Application Note ANGEN.EN005