วันนี้เราสามารถช่วยคุณได้อย่างไร?

Auxiliary contacts of thermal-magnetic motor circuit breakers

The auxiliary contacts which overall function for motor breaker for TeSys GV2, TeSys GV2L, TeSys GV3  and TeSys GV3L

Tesys GV
(1) - Choice of N/C or N/O contact operation, depending on which way round the reversible block is mounted.