How do I perform the meter PM8000 series resets using the display.
You can perform the meter resets using the display after entering a valid password and the meter resets will clear the meter’s onboard data logs and related information.
Notice: the user must be ensured all important data from the device has been retrieved before performing a reset.
You may following the step below to do the meter resets
Notice: the user must be ensured all important data from the device has been retrieved before performing a reset.
You may following the step below to do the meter resets
- Press the Home button on the display.
- Navigate to Setup Menu > Resets.
- Press Select.
- Press Edit. Enter your meter’s password, if prompted. (Default password is 0)
- Press the up or down icons to navigate available resets. A gray bar appears behind the active selection.
| Reset | Description |
|---|---|
| Master Reset |
|
| Peak Demand Reset | Clears meter peak demand values. NOTE: The peak demand reset has a lockout period that sets the minimum time allowed between consecutive resets. |
| Min/Max Reset | Clears all accumulated maximum and minimum values stored in the meter. |
| Digital Input Count Reset | Clears the digital input status change counters. |
| Harmonics Min/Max Reset | Clears all accumulated maximum and minimum harmonics values stored in the meter. |
| Disturbance Count Reset | Clears the sag/swell event counter. The sag/swell event counter counts the number of sag/swells that have occurred since power-up or the last reset to provide power quality information to energy management systems. |
| EN50160 Reset | Clears all EN50160 parameters and statistics accumulated in the meter. |
| Option Modules Reset | Resets communications to expansion modules connected to the meter. |
- Press the up and down buttons simultaneously.
- Press Select to accept the change.
- Press Select to confirm.