VPL06N SPL alert แก้ไขอย่างไร
One or more steps have fallen below 75% of initial power: risk of resonance for capacitor bank with the detuned reactor.
Step number and error code will flash alternately. Steps identified as "SPL" are moved to Fix Off.
Solution
1. Check step (Step No. will illuminate)
2.The issue step will below 75%
3.Chang or disconnect the issue step
4. Reset step database (Go to set up menu -> Pin 242 -> 600 -> 602 -> YES)
5. Auto step (AI YES)
6. SPL will appear
User Manual
https://www.se.com/ww/en/faqs/FA363433/