Issue
Is ProWORX 32 supported on Windows Server 2003, 2008 or 2012 operating systems?
Product Line
ProwORX 32
Environment
Windows 7, Windwos 10
Resolution
ProWORX 32 is not qualified to run on Microsoft Windows Server 2003, 2008 or 2012 operating systems.
Yayımlanma amacı:Schneider Electric Turkey