{}

SSS'leri Arayın

{"searchBar":{"inputPlaceholder":"Anahtar kelimeye göre arama yapın veya soru sorun","searchBtn":"Arama","error":"Lütfen aranacak bir anahtar kelime girin"}}

What is the use of favourite page in PM1130H meter ?

The PM1130H meter allows you to select 3 parameters and arrange them in required order to
be displayed in favourite page. These parameters can be selected only through
communication and are based customer requirements. Some parameter logs are
of utmost importance and navigating to those parameters takes time. For ease of
navigation and accessibility, the meter allows you to chose 3 parameters and lock
the page for easy reading. The selectable parameters are:
• V L-L
• V L-N
• A
• F
• W
• PF

Schneider Electric Turkey

Bu yardımcı oldu mu?

Schneider Electric Türkiye ile İlgili Ürünler
Schneider Electric Türkiye ile İlgili Ürünler