{}

Markalar

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Web Sitesine Hoş Geldiniz

Web sitemize hoş geldiniz.

SSS'leri Arayın

Osisense XG_Reliability data of the XGCS491B201 RFID panel mounting smart antenna 13.56 MHz : MTTF ...

The reliability data of the XGCS491B201 RFID panel mounting smart antenna 13.56 MHz, are the following :
- MTTF = 185 years (mean time to failure), supply every day, 24 hours per day.
- MTTFD =  370 years (mean time to dangerous failure),
- DC = 0 (diagnostic coverage) of the RFID smart antenna,
- mission time = 20 years.
They are used for the functional safety, according to the ISO 13849-1 standard (Performance Level).
The MTTF calculation is made according to the IEC 62380 standard, value for 30°C temperature.

Schneider Electric Turkey

Schneider Electric Türkiye ile İlgili Ürünler
Schneider Electric Türkiye ile İlgili Ürünler