This user guide provides instructions for installing, configuring, and using the Shutdown Wizard software, a specialized UPS management platform designed for SNMP Manager. The document covers system requirements, installation procedures, startup methods, and uninstallation steps. Shutdown Wizard focuses on shutdown command functionality and operates with UDP service on port 31234. The software is compatible with various Windows operating systems including Windows 2000/2003/2008/2012/2016/2019 and Windows XP/Vista/7/8/8.1/10 in both 32-bit and 64-bit versions. AI-assisted summary (Full document authored and validated by Schneider Electric experts).
檔案
| 檔案名稱 | |
Shutdown wizard user manual (SE) (1).pdf |