{}

搜尋常見問題

{"searchBar":{"inputPlaceholder":"使用關鍵字搜尋或提出問題","searchBtn":"搜尋","error":"請輸入搜尋關鍵字"}}

How do I program the U10XARR001210 Ulti RF Repeater?

RF Repeater Programming Procedures

ID Recognition or Programming Procedure
1. Select the Function Selector at the back of the Handheld (HH) Remote to the “Program” position.
2. Press the Program button on the Repeater until the Program LED turns on.
3. Press any Scene or Device Key on the HH Remote to complete the ID recognition programming.
4. The program LED on the Repeater will turn off.
5. Exit program mode for the HH remote.
Remarks : The RF control range during programming will be around several meters which is shorter than that during normal operation.
ID Delete Procedure
1. Select the Function Selector at the back of the HH Remote to the “Program” position.
2. Press the Program button on the Repeater until the Program LED turns on.
3. Press any Scene Key on the HH Remote to be deleted (but make sure that HH Remote should already been programmed).
4. The program LED on the Repeater will turn off.
5. Exit program mode for the HH remote.
Remarks : The RF control range during ID delete will be around several meters which is shorter than that during normal operation.
Clear Procedure
1. Press and hold the Clear Button on the Repeater for 3 seconds.
2. The Program LED will flash 3 times and the remote ID memory of the Repeater has been cleared.
Testing Procedure
1. Press the Test Button on the Repeater.
2. Transmit LED will flash when “Test” key is pressed. Press the “Test” key will transmit a specific repeater command code to turn on the wall switches. The number of transmission is dependent
on the number of pre-programmed remote control (e.g. if there has 3 different remote ID being programmed into the repeater, each press of “Test” key will transmit 3 times of the command).
Press again of the “Test” key will transmit “All Off” command to the wall switches. 3rd press of “Test” key will transmit repeater command, and so on. By trial and error, the user can determine the
right position to locate the repeater.
Repeater Number selection Procedure
A maximum of 5 Repeaters can be installed in one house. Each Repeater should be set with different Repeater Number within one house. The Repeater Number indicator (Only one of the five LEDs will
light up at the same time) will indicate the Repeater Number by lighting up the LED indicator in different position.
1. Press the Select Button on the Repeater.
2. The Repeater Number indicator will swap to the next position. (Swap sequence: 1, 2, 3, 4, 5, 1, 2…)
Press the Select Button until the Repeater Number indicator is in your desired position.


Pleaase note that this product is no longer commercialised.

這是否有幫助?