If RegisterType is m/M, then optional field for scaling and offset looks like
size:scale:[lowerBound:]upperBound;O:offset
The lowerBound and upperBound must be entered in hexadecimal format.
For more information on optional fields, refer to the PowerLogic G3200 Modbus-to-IEC 61850 Server User's Manual, PLSED309028EN.