常見問題 (FAQs)

About the measurement unit of Flusarc_36, can any current transformer reach both metering & protection classes in one same core?

公佈日期: 25 二月 2016

We confirmed that the proposed CT can reach both metering/protection classes, we could propose:

Um=0.72/3kV                 Ext=120% Ith=25kAx1s       F= 50Hz          Norme: IEC61869-2
AOL1/N2 200/ 1-1A      10 VA Cl. 0,5 FS<=10         2.5 VA 5P10 + 0.5 NO F.S.
                                                    core 1                                         core 2

The only limitation is we are not able to reach the F.S. for metering class in this core.

對您是否有幫助?

我們如何進行信息改進?

找不到想要的答案?

歡迎聯絡客戶服務團隊,接收有關技術支援、投訴協助等資訊。