我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Reject: it Is it possible to use the up and down arrow key on ATV61/71 drive to act as + and - speed?
Issue:
ATV61 can I set the up / down arrow buttons for  + /- speed?

Product Line:
Altivar Machines, Altivar 61, Altivar 71

Environment:
All models and serial numbers

Cause:
Installation / Setup

Resolution:
No, however, in the ATV61 or ATV71  Command Menu / F1 - F4 Key Assignments can be configured for (+) / (-) speeds on the removable HMI.