{}

搜尋常見問題

{"searchBar":{"inputPlaceholder":"使用關鍵字搜尋或提出問題","searchBtn":"搜尋","error":"請輸入搜尋關鍵字"}}

What are the main features of EM64xxH series meter ?

The meter supports many features, a few of the features are listed below:
• LED display screen: Intuitive self-guided navigation using four buttons LED
display, with three lines of concurrent values, and load bar that indicates
current loading
• Energy accounting and balancing
• Time counter: Meter provide On hours and Load run hours to advise regarding
maintenance requirements
• Protective cover to ensure terminal screws do not detach from housing and for
safety against unintentional finger contacts with terminals
• Active, reactive, and apparent energy readings
• Cyber security: The meter enables disabling the RS-485 port through front
panel keys against unauthorized access. This feature can also be used for
toggling between the RTU devices in case of limited availability of nodes in
software system
• Measurement of True PF

這是否有幫助?