Where is the modbus serial communication port located on the Altivar Process Drive?
Issue:
Location of modbus serial communication port on Altivar Process Drive.

Product Line:
ATV600 / ATV900 series

Environment:
All models

Cause:
N/A

Resolution:
This drive has multiple RJ45 communication ports.  The Modbus Serial Communications Port is located on the control terminal card towards the right bottom.  It is labelled Modbus VP12S.
Reference picture below and document EAV64325

1 Modbus serial communication port


port

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: