Can CLI be disabled or set to 'ignore' on an ATV61/71?
Issue:
Wants to disable or ignore a CLI on an ATV61/71.

Product Line:
Altivar 71

Environment:
All

Cause:
Drive is reaching CLI

Resolution:
CLI means current limit. It cannot be disabled or set to 'ignore'.
This is a drive state not a fault. It is there to protect your motor. If the drive stays in CLI for longer than one minute, it will fault on overload.

Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: