How to automatically reset peak KW demand, current or voltage demand at the beginning of a new month in PME7 for ION meters
Published date:
30 July 2019
Issue
There may be a need to automatically reset the peak demand values for power, voltage, current at the start of a new month or a new year.
Product Line
Power Monitoring Expert 9.x
Power Monitoring Expert 8.x
Power Monitoring Expert 7.x
Struxureware Power Monitoring 7.0.x
ION 7xxx/8xxx Power Meters
Environment
Power Monitoring
Cause
In most cases, a user can only manually reset the peak demand values from the menu options in ION setup or from the front panel display of the meter. There is not an automatic demand reset capability by default on the meters.
Resolution:
The following steps display custom programming that can be set up on an ION meter or in the Virtual ION Processor (VIP) within the Designer application.
1. First create a sliding window demand module and link it to the desired measurement. To calculate demand for power, current and voltage, 3 different sliding window demand modules will be required.
2. Set the sub interval length and the # of sub intervals in setup registers and save the module. This will compute the demand value.
3. To compute the peak demand value, link the output of the sliding window demand module to the source input of a maximum module.
The output of the maximum module will hold the peak demand value for the measurement linked to the input of the sliding window demand module.
4. To set up an automatic reset of the peak demand module, link the reset input of the maximum module to the desired pulse output of a clock module.
Linking the reset input of the maximum module to the "New Month" pulse output of the clock module will cause the maximum module to reset at the beginning of each month.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.