How do I change the default display to show PSI on the keypad of the ATV61 or ATV71 drive?
Published date:
30 July 2019
Issue:
Display custom "User Name"
Product Line:
ATV61 and ATV71
Environment:
All models and serial numbers
Cause:
None
Resolution:
How to customize your display to show your [User Name] as PSI using the PID Feedback
Scale the AI2 to 0-20mA
From the drive menu go to 1.5 [INPUTS / OUTPUTS CFG] press enter
Go to AI2 CONFIGURATION press enter
Set AI2 Min. Value to 0
Set AI2 Max. Value to 20
From the MAIN menu go to Menu 7 – [DISPLAY CONFIG]
Select Sub-menu 7.1 – [USER PARAMETERS]
Go to [PARAMETER SELECTION]
Go to sub-menu 1.2 [MONITORING]
Select [PID feedback] (a checkmark will appear in the box)
Press the (ESC) button 2 times
Go to [CUSTOMIZED SELECTION]
Select [PID feedback]
Select [User name]
Rename the parameter using the thumbwheel
Turn the thumbwheel clockwise to “P” then press “F3”
Turn the thumbwheel again to “S” then press “F3”
Turn the thumbwheel again to “I” then press “ENTER”
Press (ESC) back to the main menu.
Go to Menu 6. [MONITORING CONFIG.]. Press “ENTER”
Go to [MONITOR SCREEN TYPE]. Press “ENTER”
Go to [PARAMETER SELECTION]. Press “ENTER”
Scroll down to the newly named parameter “PSI”, Press “ENTER”
Press the (ESC) button
Multiplier = 100
Divisor = 16
Press the ESC button until the display shows “PSI”
Make the your [User name] as the default display
Enter menu 6. [MONITORING CONFIG] from the MAIN MENU
Enter menu 6.2 [MONITOR SCREEN TYPE]
Enter [PARAMETER SELECTION]
Select your [User name] parameter from the list of parameters (Note: a maximum of two parameters is allowed. You may need to unselect a parameter in order to select your [User name]”
Press ESC 4 times to see your [User name] displayed on the HMI.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.