{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Which operating system is Unity Pro version 10 compatible with?

Unity Pro version 10 is compatible with the following os:

Windows 7 32/64bits
Windows 8 32/64bits
Windows Server 2012

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.