Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
What is the minimum speed of rotation for Lexium Integrated Drives of the ILE type (Brushless DC motors)
The minimum speed for ILE1x devices is 300 rpm's, while the minimum speed for ILE2x devices is 60 rpm's
This is because the newer design ILE2x types have improved signal evaluation of the internal position feedback.
Speeds lower then the minimum are possible but the motion will be non-continuous motions. (stepping rotation)
It should be noted that ILE devices only have 12 encoder points per rotation, therefore speed regulation is not very good.
ILE devices are designed and intended for use for position applications such as format adjustment application and should not be considered for applications in which precise speed of movement is critical.
rev 11-20-18
This is because the newer design ILE2x types have improved signal evaluation of the internal position feedback.
Speeds lower then the minimum are possible but the motion will be non-continuous motions. (stepping rotation)
It should be noted that ILE devices only have 12 encoder points per rotation, therefore speed regulation is not very good.
ILE devices are designed and intended for use for position applications such as format adjustment application and should not be considered for applications in which precise speed of movement is critical.
rev 11-20-18
Did this answer your question?
Explore more
Range:
Explore more
Range: