Browse FAQs

What are the part numbers for the connector kit of ATV340 drives?

Published date: 11 December 2019

Issue:
Is the connector kit available ATV340 drives?

Product Line:
ATV340, Altivar 340

Environment:
All

Cause:
N/A

Resolution:
Yes, the part numbers are listed below:
Size 1 = VW3A34001
Size 2 = VW3A34002
Size 3 = VW3A34003

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.