{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

How do we update PLC Symbols linked in EcoStruxure Operator Terminal Expert (formerly known as Vijeo XD)?

Issue:
There is no option in EcoStruxure Operator Terminal Expert (formerly known as Vijeo XD) to update PLC symbols already linked in the application.

Cause:
The feature to update the symbol link has not been implemented yet in EcoStruxure Operator Terminal Expert. It will come in a future release.

Environment:
Vijeo XD 3.0.x, EcoStruxure Operator Terminal Expert 3.1, 3.2

Resolution:
For the time being, until the feature is implemented, please delete the symbol link and re-link the file each time there is an update for the PLC Symbols.

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.