Browse FAQs

Where do I download EcoStruxure Machine Expert Basic?

Published date: 12 August 2019

Issue
Where do I download the EcoStruxure Machine Expert Basic v1.0 PLC configuration software installer?

Product Line
EcoStruxure Machine Expert Basic

Environment
Windows 8, Windows 10

Resolution
The download link for the installer for EcoStruxure Machine Expert Basic v1.0 can be found on this webpage:
https://www.se.com/ww/en/download/document/Machine_Expert_Basic/

This software can be used to program the Modicon M221 line of PLCs and is the successor to SoMachine Basic v1.6 SP2 moving forwards. Project files from SoMachine Basic can be automatically migrated to EcoStruxure Machine Expert Basic by simply opening the .smbp extension files in EcoStruxure Machine Expert Basic.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.