How to resolve the error "I2C communication error" on the HMIG5U/HMIG5U2?
Published date:
01 August 2019
Issue:
When powering up the HMIG5U/HMIG5U2, there is an error at the bottom of the screen (when the Schneider Electric logo is displayed) that states "I2C communication error".
Product Line:
HMIG5U, HMIG5U2
Resolution:
The "I2C communication error" appears when the connection from the HMIDT to the HMIG5U/HMIG5U2 is distorted or bad. Check the pins on the back of the HMIDT and the pins on the HMIG5U/HMIG5U2 to ensure there is no rust, corrosion or bent pins.
Removing and reattaching the screen usually resolves this issue.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.