{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the dimensions for the empty Easy9 Multirow Compact Consumer Unit range of consumer units?
Refer to the image and table below for the detailed dimensions:
Easy9 Multirow CCU showing the dimensions
Easy9 Multirow CCU Dimensions
Reference No.TypeUsable WaysHeight H (mm)Width W (mm)Total Depth D (mm)
EZ9E212MCCU Standard 22522.4312111.7
EZ9E312MCCUStandard34780.4312111.7


Also, we do have CCU of 1 row with several variants.
You can find the dimension details and other information in the catalogue
Refer the below link of the range for more details. https://www.se.com/uk/en/work/products/product-launch/easy9/

Schneider Electric UK

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: