{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Acti9 Isobar & Isobar P Spare Links

This is the part number for the links SEA9PNPB250TB.  These are only compatible with Acti9 Isobar P distribution boards.
This part is for the older ISOBAR boards, not the Isobar P SEA9NPB250TB
This reference SEA9BINCKIT is the kit for the straight copper busbars this can be used in both boards.

Schneider Electric UK

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: