Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Integrated digital display module, Twido, optional for PLC, left side mounted

TWDXCPODM

Recommended replacement(s)

TWDXCPODM is replaced by:
EAN Code: 3595862044486
"They are the basic elements of Premium multirack configurations"
"They enable all the modules of a PLC station to be fitted"
"Have standard and entendable racks"
"A double format processor module is always installed in it"
"They can be mounted in cabinets, machine frames or on panels."