• Default Alternative Text

    Better connected operations

    Improve safety, efficiency, and productivity at every stage — from shop floor to top floor.

  • Worker using touch screen machine controller
    “I want to easily access the right info to safely operate on target.”

    Our Magelis HMI range is designed for fast deployment and ease of use:

     - Instant mobility: With one wireless display, you can access other HMIs on the network

     - Instant access: From the HMI, you can directly visualize our Modicon PACs and Altivar Process drive web servers

     - Intuitive, multi-touch navigation: No need for extra training.

  • Male workers using a laptop near an oil well, oil and gas, energy management  
    “I want to maximize productivity by reducing unplanned downtime.”

    Our SCADA Expert ClearSCADA in combination with the SCADAPack RTUs, Realift controllers, and Accutech wireless sensors reduce the impact of unplanned downtime:

     - Built-in intelligence of our Realift controllers: Proactive mitigation of conditions that could lead to unplanned downtime events

     - Real-time alarming: Instant notifications of unplanned downtime events

     - Operational visibility: Access to the information to troubleshoot/resolve the condition causing the event.

The Chat is available now