United Kingdom
Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website for company information.

Select your location
  • Default Alternative Text
    Intelligent control for Oil & Gas operations

    Pump & Motor Control Solutions

    As energy demands grow and environmental and safety regulations increasingly impact Oil & Gas industries, energy-efficient operations and lower maintenance cost are key. Oil & Gas players face a global resource challenge and the rising costs of energy and raw materials plus decreasing numbers of skilled employees. To ensure safety, security and reliability while protecting your bottom line, you need intelligent solutions to monitor, control and optimize your assets.

  • Read

    • Read more about Schneider Electric solutions

      Altivar 61 and Altivar 71 Drives

      Schneider Electric Altivar™ Plus enclosed drives feature the Altivar 61 and Altivar 71 adjustable-frequency drives providing a robust, packaged, adjustable-speed solution for commercial, industrial, and municipal applications. These drives combine the reliability and ease-of-use of the Altivar drives family with proven, validated, and tested drive system designs Read More
    • Read more about Schneider Electric solutions

      The Altistart 01 Soft start

      The Altistart® 01 soft start enhances starting performance by ensuring a smooth and controlled start for asynchronous motors, while providing torque surge suppression during both the starting and stopping operation. This highly functional mini soft start can help to decrease your maintenance work and production downtime by preventing the mechanical shocks that create wear and tear on your motor and machinery.

      Read More
    • Read more about Schneider Electric solutions

      Well-Guard Control Pumping Plant Panels

      The most complete, dependable and durable pump panel product offering available, including NEMA and IEC style motor starters (both full-voltage and reduced-voltage versions); all housed in rugged NEMA 3R outdoor enclosures. A complete line of enclosed drives and soft starts.

      Read More
    • Read more about Schneider Electric solutions

      TeSys T Motor Management System

      TeSys T is an advanced motor management and protection system designed to prevent malfunctions. Both motor and mechanics are protected, so unexpected process or production halts can be anticipated.

      Read More
    • Read more about Schneider Electric solutions

      The Altistart 22 soft start

      The Altistart® 22 soft start is designed for 3-phase AC motors and standard applications with true 3-phase control. It has an integrated by-pass contactor for compact design, reduced wiring time and low heat dissipation.

      Complete motor-/starter-/application protection Integrated Modbus communication

      Read More
    • Read more about Schneider Electric solutions

      The Altistart 48 soft start

      The Altistart® 48 soft start is designed for 3-phase AC motors and harsh applications (starting time >30s). Its patented torque control system (TCS) manages soft start and dynamic breaking with motor thermal protection and motor preheating functions. It also has the following features:

      Machine under- and overload protection Cascaded starting and deceleration of a number of motors Integrated Modbus communication and other gateway solutions Large number of configurable I/O Automatic restart Plug and play factory settings

      Read More
    • Read more about Schneider Electric solutions

      The Altivar 1260

      The Altivar® 1260 – is a range of medium voltage variable frequency drives from 700 to 7,500 HP, available in 3.3KV or 4.16KV output voltage ratings. The flexible, high performance drive is ideally suited for large pump, fan and compressor applications and complements Schneider Electric’s broad portfolio of bundled power solutions, including distribution gear, MV Soft Starters, plant equipment and services.

      Read More
    • Read more about Schneider Electric solutions

      Taco, Inc., Cranston, Rhode Island HVAC pump manufacturer meets customer demand and captures sales with new drive offerings.

      Taco, Inc., America’s leader in hydronic systems for residential and commercial building applications, was established in 1920. A third-generation family-owned company, Taco’s corporate headquarters are located in Cranston, Rhode Island, with manufacturing facilities in both Cranston and Fall River, Massachusetts.
      Numerous industry initiatives have been put in place to provide building owners with assistance and incentives to incorporate energy savings in both new and existing buildings, including the LEED® green building certification system developed by the U.S. Green Building Council, the EPA’s Energy Star program, and the emerging Smart Grid efforts. As of August 2011, more than 1.5 billion square feet of commercial space was LEED-certified. As a result of the increased energy focus, Taco, Inc. found more and more customers requested variable frequency drives (VFDs) in addition to their pumps. In 2009, Taco approached Schneider ElectricTM about selling open drives. Additionally, they were considering selling a pump with a mounted drive for its smaller horsepower series. Read More

The Chat is available now