United Kingdom
Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website for company information.

Select your location
  • Default Alternative Text
    For hospitals, data centers, industrial process facilities, etc.

    MISSION-CRITICAL STANDBY GENERATOR DEDICATED SOLUTION

Default Alternative Text

Challenges

Protecting and switching standby generation in mission critical facilities

Hospitals, data centers, and other critical facilities must operate 24/7. The most important characteristics of their power systems are availability, reliability and security. They rely on generators to keep running in case of an outage, which must respond and recover quickly under any conditions.

Our experts help you throughout the entire generator life cycle

Illustration, Machine LifecycleSolutions, Industrial production, machine control.
  • Solutions

    • Continuity: Compact or Masterpact breaker with Micrologic trip unit offers measurement and diagnostics.
    • Avoid cutoff during transfer: Genset circuit breaker and switch resists sum of short-circuit currents, allows selectivity, while ensuring there is no interlocking.
    • Parallel genset coupling: Increases standby power, compensates for unavailability of generator.

The Chat is available now