Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.

Schneider Electric Announces Enhancements to Core VisiPacT Heavy Duty Safety Switch Amplifying Quality & Productivity

Boston, MA, USA

19/06/2023

  • Includes new features and accessories to meet new national electrical codes
  • Enhanced safety and performance based on Voice of the Customer (VoC) recommendations
  • Offers QR code for quick access to safety switch information
  • Designed to outperform other switches in a wide range of demanding applications
  • Power isolation solutions for daily activities and emergencies

Boston, MA, June 19, 2023Schneider Electric, the leader in digital transformation of energy management and automation, today released a new version of its flagship Square D safety switch offer, VisiPacT heavy duty safety switch, bringing new features and refreshed design to the trusted offering.

Designed for long-term durability to improve safety and productivity, the new VisiPacT heavy duty safety switch (30-200A) is setting the standard for performance, quality, and reliability in today’s commercial and industrial applications. This latest evolution includes enhancements based on feedback from Schneider Electric customers, including new standard features such as a viewing window, hook stick handle, QR code for quick access to information, touch safe barriers and more.

The updated VisiPacT heavy duty safety switch includes the following new features:

  • Standard viewing window for visual verification of switch position without the need to open the door: Maintenance personnel can visually inspect the switching mechanism and fuses without opening the cover or turning off power to the load, which increases safety and efficiency dramatically.
  • New ergonomic handle to accommodate hook stick for safer operations: Adds an extra layer of safety when exercising the switch, allowing first responders and electricians to stand outside the arc boundary to operate the switch when necessary.
  • QR code for quick access to safety switch information: Maintenance workers and electricians can access pertinent information on the safety switch using a QR code such as critical ratings, mechanical parts, wiring diagrams, manuals and instruction bulletins.
  • Touch safe barriers to prevent accidental contact: Tested to IP20 standards for optimal performance and safety.
  • Allocated spacing for customer-required labeling: Label information, such as naming the load (Pump 1, AC Motor, etc.) and/or Arc Flash Hazard information can be added easily in the allocated space.

“VisiPacT heavy duty safety switches represent the next evolution in a product line with a vast history of providing a safe means of disconnect in both commercial and industrial settings,” said Justin Siefkes, Vice President of Energy League at Schneider Electric. “In fact, VisiPacT has a field-proven, time-tested switching mechanism that our customers requested remain the same due to its reliability and performance.”

Safety switches are critical to the safe and profitable operation of power devices and other equipment such as motors, HV/AC, pumps, and fans (NEC article 430.102B) in all commercial and industrial operations. In addition, organizations such as OSHA and NFPA have recently increased and modified requirements for safety switch use.

With more than 130 years of Square D safety switches setting the standard for safety, VisiPacT heavy duty safety switch provides significantly higher levels of mechanical endurance than NEMA KS-1 life test requirements. In fact, the standard for the design life of VisiPacT is a minimum of three times the NEMA requirement, which is important for long-term safety and reliability.

“With safety, reliability, sustainability and innovation at our core, we’re excited to provide our customers with an enhanced solution that addresses their long-term power supply and isolation needs for commercial and industrial buildings,” said Justin Siefkes, Vice President of Energy League at Schneider Electric.

VisiPacT will be in our Schneider Electric booth at the NFPA Expo (booth #1339 in the Electrical Safety Pavilion). 

For more information, please visit here.

-    ###   -

About Schneider Electric

Schneider’s purpose is to empower all to make the most of our energy and resources, bridging progress and sustainability for all. We call this Life Is On.

Our mission is to be your digital partner for Sustainability and Efficiency.

We drive digital transformation by integrating world-leading process and energy technologies, end-point to cloud connecting products, controls, software and services, across the entire lifecycle, enabling integrated company management, for homes, buildings, data centers, infrastructure and industries.

We are the most local of global companies. We are advocates of open standards and partnership ecosystems that are passionate about our shared Meaningful Purpose, Inclusive and Empowered values.

Adoption of Wiztrust's Blockchain Certification Platform

From October 2nd, 2019, in order to secure its communication, Schneider Electric certifies its contents on Wiztrust. You can check the authenticity on the website Wiztrust.com for Corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page: