Browse FAQs

What is the stand alone AIC withstand rating of a 2510F?

Published date: 26 June 2020

Issue:
AIC rating of a 2510F

Product Line: 
Nema Starters

Environment:
2510F Manual Starter

Resolution:
1,000 amps as this is a 1hp maximum at 300V maximum starter.
Note: Stand alone rating is not to be confused with short circuit rating which is provided by the up stream protective device. (i.e. fuses, circuit breaker).

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.