Browse FAQs

What is the coil resistance on a 8501KPDR12V51?

Published date: 29 June 2020

Issue:
Coil resistance value for 8501KPDR12V51 relay

Product Line:
Relays and Timers

Environment:
8501 Type K Universal Relays

Resolution:
Coil resistance for a 12 VDC coil @ 20 degrees C +/- 10 % is 110 ohms.


CTA-ID : 2005864

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.