Browse FAQs

Are there hinges on the LDB painted wireway?

Published date: 17 June 2020

Issue:
Hinges for the LDB wireway.

Product Line:
Wireway.

Environment:
Maintenance.

Resolution:
Yes. The covers are hinged on all sizes up to 10 x 10. The 12`` x 12`` wireway is screw cover only.


CTA-ID : 2006716

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.