Browse FAQs

Can a 400A HCM panel with a vertically mounted LAP36400 main breaker, be converted from bottom to top feed?

Published date: 08 June 2020

Issue:
What needs to be done in order to convert from bottom to top feed in a 400A HCM panel with a vertically mounted LAP36400 main breaker?

Product Line:
I Line panelboard

Environment:
Installation /Application

Cause:
Clarification

Resolution:
The conversion can be done by doing the following:

1. Rotate entire interior panel assembly 180 degrees.

2. Replace factory installed Main breaker with a new top-feed LAP36400MT breaker. 

3. In some cases, the Main breaker cover plate (part of interior deadfront) must also be rotated 180 degrees to achieve proper orientation of deadfront labels.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.