Browse FAQs

What lever arm can be used for a XCKJ10553 that would be 7.6" long?

Published date: 09 June 2020

Issue:
Part number of lever arm for XCKJ10553

Product Line:
Limit Switches

Environment:
XCKJ Limit Switches

Resolution:
ZCKY59 lever can be used for lengths up to 8.4 in long. It is plastic, not steel. However, a customer supplied steel rod 1/8 in diameter could replace the plastic on the XCKJ10553.


CTA-ID : 2007546

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.