Browse FAQs

What is the difference between the 9007 MA18 and MA18S?

Published date: 17 June 2020

Issue:
Checking on the difference between the 9007 MA18 and MA18S.

Product Line:
NEMA Limit Switches

Environment:
9007C Limit Switches

Resolution:
9007 MA18 is cast zinc and the 9007 MA18S is flat steel.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.