Browse FAQs

Will the GV3A08 or GV3A09 fault indicating contact change states if we actuate the push-to-trip button?

Published date: 22 June 2020

Issue:
Functioning of the push-to-trip button on GV3 fault indicating contacts.

Product Line:
Motor Starters and Protectors

Environment:
TeSys GV Manual Starters and Protectors

Resolution:
Yes, the contacts change state just as if the starter had experienced a fault.


CTA-ID : 2007949

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.