Browse FAQs

What are the input/output specifications for a SDM350082 power supply?

Published date: 29 June 2020

Issue:
Input/output specifications for a SDM350082 

Product Line:
 Power supply

Environment:
Installation / Setup

Resolution:
Input Voltage = 105 - 125 Vac, Output Voltage = 15 Vdc, Output Current = 900mA


CTA-ID : 2007851

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.