Browse FAQs

What is the GV2L__ manual starter?

Published date: 29 June 2020

Issue:
Description of the GV2L manual starter line.

Product Line:
IEC Contactors and Starters

Environment:
TeSys GV2L Manual Starters

Resolution:
It is just like the GV2P__ but it gives the user ONLY magnetic protection. There is no thermal protection with this unit. It should be used in combination with a starter with thermal overload protection for best protection of motor circuits.


CTA-ID : 2009790

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.