{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What size lettering is used on 9001KN legend plates?
Issue:
What is the size lettering for the 9001KN 30 mm legend plates?

Product Line:
Push Buttons and Operator Interface

Environment:
30mm accessories

Resolution:
The lettering size will vary according to the size of the plate and the length of the words.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.