Browse FAQs

Does the 9050JCK Timer meet Class 1 Divison 2 applications?

Published date: 11 June 2020

Issue:
9050JCK timers suitable for class 1 div 2 applications?

Product Line:
9050JCK plug-in timers 

Environment:
Square D General Purpose Plug-in Timers 

Resolution:
9050JCK timers do not meet Class 1 Division 2 requirements.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.