Browse FAQs

Is the 2511M reversing manual starter offered in a NEMA 7 & 9 enclosure?

Published date: 30 September 2019

Issue:
Explosion proof enclosure

Product Line:
Class 2510, Class 2511 Manual Starters and Switches

Environment:
Type M and T—Integral Horsepower

Resolution:
No, they are not available in a NEMA 7 or 9 enclosure.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.