Browse FAQs

The sealed consumption listed in the Tesys U-Line catalog (8502CT0201) for 110-240 volts indicates the sealed current for the 32 amp base is less than the the sealed current for the 12 amp base. Is this correct or inverted?

Published date: 11 June 2020

Issue:
Tesys U coil consumption

Product Line:
TeSys™ U Open Motor Starter

Environment:
IEC Style Contactors and Starters 

Resolution:
Consumption values are correct as outlined.

As it may seem odd that the 32 amp base consumption is 20 mA while the 12 amp base is 30 mA, this is due to the use of a chopped voltage supply that deals with voltage adaptation followed by a current regulator which adjust the magnet dynamics.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.