Browse FAQs

What is the pinout for ATV58 Power Suite cable?

Published date: 11 June 2020

Issue:   
ATV58 power suite cable pinout.
 
Product Line:   
ATV58
 
Environment:  
All
 
Cause:  
Cable VW3A8106 pinout
 
Resolution:   
The cable is a basic Ethernet patch cable and do not have the pinout.

The solution is to get the cable kit VW3A8106 which has all the necessary components for connection to the unit.

If customer has a 9-pin to 9-pin RS485/232 converter, the cable is straight through from the converter to the laptop.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.