Browse FAQs

What is the Start-Stop Pushbutton kit for the definite purpose enclosed starters?

Published date: 24 June 2020

Issue:
What is the Part Number for the Start-Stop Pushbutton for the 8911DSG & 8911DPSG NEMA 1 Enclosed Starters?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Definite Purpose Starters

Resolution:
As outlined below: (Note: Class 8911DPS starters are not supplied with holding circuit contacts, therefore the use of 9999D10 auxiliary contact is required with this control station kit.)

For Compact 20, 25 & 30 amp Type DS*: Not available.
For Type DPS* 20 amp through 40 amp devices: 8911DPB1.
For Type DPS* 50 amp devices : 8911DPB1 & 9999BLX bracket.
For Type DPS* 60 amp through 90 amps devices: No kit available, suggest the use of 9001 Type K control station(s) mounted in the side of the enclosure.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.